Skip to main content
AGome.7
Associate II
June 7, 2023
Question

Issue with VL6180X returning incorrect value when reading the RESULT__RANGE_RETURN_CONV_TIME register.

  • June 7, 2023
  • 2 replies
  • 1280 views

So from my understanding, after polling the sensor we can read directly from the RESULT__*** registers to reveal things such as distance, return rate, error code and such to view the results from the sensor range measurements. However, I've seen that when reading the RESULT__RANGE_RETURN_CONV_TIME register, it returns the same number, 16777215 microseconds (0x00FFFFFF). This number should be waaaay smaller that (below the Max_Convergence_Time threshold), and it should also change based on the target's distance and reflectance.

Below I have a snippet of a terminal printing out values from a ToF sensor's measurements. I used my hand as a target and waved up and down perpendicular to the sensor in an attempt to see a change in the convergence time, but as we can see it stays the same.
_legacyfs_online_stmicro_images_0693W00000dDK9j.png 

Is there something I am missing?

This topic has been closed for replies.

2 replies

Zhiyuan.Han
Technical Moderator
June 8, 2023

Hi

I did same test, the rtnConvTime should not be a constant value. I was using API to read all the ranging result.

Inside _GetRateResult(dev, pRangeData) function, there is a ReadDword function for RESULT_RANGE_RETURN_CONV_TIME.

 status = VL6180_RdDWord(dev, RESULT_RANGE_RETURN_CONV_TIME, &m_rtnConvTime);

distance=36; status=0; ambient=270; rtnConvTime=155

distance=33; status=0; ambient=120; rtnConvTime=150

distance=30; status=0; ambient=232; rtnConvTime=155

distance=30; status=0; ambient=160; rtnConvTime=150

distance=30; status=0; ambient=116; rtnConvTime=154

distance=27; status=0; ambient=394; rtnConvTime=152

distance=24; status=0; ambient=77; rtnConvTime=154

distance=24; status=0; ambient=193; rtnConvTime=155

distance=24; status=0; ambient=278; rtnConvTime=151

distance=18; status=0; ambient=0; rtnConvTime=151

distance=18; status=0; ambient=348; rtnConvTime=155

distance=15; status=0; ambient=157; rtnConvTime=152

distance=15; status=0; ambient=148; rtnConvTime=162

distance=15; status=0; ambient=111; rtnConvTime=162

distance=12; status=0; ambient=389; rtnConvTime=154

distance=9; status=0; ambient=270; rtnConvTime=155

distance=9; status=0; ambient=259; rtnConvTime=162

distance=9; status=0; ambient=194; rtnConvTime=154

distance=6; status=0; ambient=111; rtnConvTime=162

distance=6; status=0; ambient=272; rtnConvTime=154

distance=6; status=0; ambient=194; rtnConvTime=154

so suggest you check I2C Dword read/write functions.

Br

Zhiyuan.Han

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
AGome.7
AGome.7Author
Associate II
June 8, 2023

Yea, I figured out my issue, and it was related to the I2C Dword read/write functoins. In my setup, I am using an I2C to Serial ftdi chip to communicate to the ToF sensors using my computer. Issue was that the driver was incorrectly setting the ACK bit in between reads from the sensor's 32bit registers, so it resulted in bad data. I fixed it and it's now returning valid rtnConvTimes. Thanks for the suggestion!