measure target through a tube
I can see from the datasheets (VL53L4CD for example) that the emitter and sensor volume is represented as two cones that start at the sensor face and grow bigger as the distance from the sensor increases.
If I am measuring the distance to a target that is visible through a "tube", can the sensor figure out that the walls of the tube are not the target and ignore them, or do I need to ensure that the tube diameter is larger (+ some margin) than the diameter of the sensing element's "cone" as shown in the datasheet?