Please explain the optical center values returned by ST's VL53L1X API function VL53L1_GetCalibrationData()
I am using Pololu's adaptation of the ST library for Arduino. When I call VL53L1_GetCalibrationData() and print the optical center x and y values, I get 0x70 for both. How should I interpret this value? I've tested on an Arduino Uno as well as a MKRZERO. I was expecting these values to be in the range 0x00 .. 0x0F since the SPAD array is 16 X 16. Is nibble order simply reversed? If so, should one reverse the nibble order when identifying a SPAD for other API functions, e.g. VL53L1_SetUserROI()?