Problem in changing address of VL53L1 sensors using "VL53L1_SetDeviceAddress" function.
Hi ST team and community,
I'm here because I have some troubles on the process of initialization of multiple sensors VL53L1.
I use the library of VL53L1.
The process is the following :
- Shut down reset pin XSHUT of each sensor
Then, in a loop (to setup my 2 sensors) :
- Power ON the first sensor with XSHUT pin.
- Trying to change address using "VL53L1_SetDeviceAddress" function.
Then, switch to another sensor in the loop until initialization of my 2 sensors.
My problem is when the loop arrives on the"VL53L1_SetDeviceAddress" function it gets fail.
Question is, When I try to connect 2 sensor and go for to change address it get fails.
Note: If I remove second sensor and dis-connect XSHUT pin from host of 1st sensor and attach it to pull up by connecting 10k it works and I'm getting data with default address.