Skip to main content
Abu Ziyech
Visitor II
February 10, 2022
Question

[Proximity Sensor ADC with DMA Problem] I have GP2Y0A41SK0F Sharp for distance measuring sensor. the datasheet says it needs 16.5 ms with 3.7 ms tolerant. for sampling time. So I assumed I need to configure PCLK2 (I use ADC2), ADC Clock Prescaller, .

  • February 10, 2022
  • 1 reply
  • 893 views

channel sampling, then calculate those parameters until 16.5 ms found. The problem is kinda impossible to get 16.5 ms even I tried to adjust those parameter. anyone has a clue? Iam using STM32F407VGx

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
March 28, 2022

I'd post this to the STM32 community. If you post it to the Time-of-Flight group the only thing you will get is a suggestion that you should have used an ST Time-of-Fight rather that that Sharp device.

(Just kidding, but I don't know enough about the STM32 and Sharp to be useful to you. Try the STM32 page.)

  • joh