Reading several VL53L7CX sensors with a Nucleo
Hello everyone,
I am trying to read data from three SATEL-VL53L7CX, using only their mini-PCB part, with a Nucleo F401RE.
To do so, I did the following wiring:
- each sensor is using a different I2C bus (sensor 1 is plugged on SDA1/SCL1, sensor 2 on SDA2/SCL2, etc)
- the GND of each sensor is connected to the Nucleo’s mass
- IOVDD and AVDD are respectively connected to 3.3V and 5V
- the LPn pins are connected to 3 different GPIO pins (D2, D4, D6)
I am using Arduino IDE to develop the code. Here it is:
/************************** INCLUDES **************************/
#include <Arduino.h>
#include <Wire.h>
#include <vl53l7cx_class.h>
#include <stdio.h>
#define DEV_I2C Wire
#define SerialPort Serial
#define LED_PIN PC13
#define TOF 3 // number of ToF
#define LPN_PIN1 3 // sensor #1 wiring
#define LPN_PIN2 5 // sensor #2 wiring
#define LPN_PIN3 7 // sensor #3 wiring
/************************** PARAMETERS **************************/
// Components.
VL53L7CX sensor1(&DEV_I2C, LPN_PIN1);
VL53L7CX sensor2(&DEV_I2C, LPN_PIN2);
VL53L7CX sensor3(&DEV_I2C, LPN_PIN3);
VL53L7CX* tab_sensor[] = {&sensor1, &sensor2, &sensor3};
// Global param.
uint8_t res = VL53L7CX_RESOLUTION_4X4;
uint8_t ranging_mode = VL53L7CX_RANGING_MODE_CONTINUOUS;
uint8_t address[] = {0x54, 0x56, 0x58}; // sensors' I2C address
uint8_t status;
/************************** MAIN **************************/
void setup()
{
// Initialize serial for output.
SerialPort.begin(115200);
while (!Serial) ;
SerialPort.println("------- BEGIN INITIALISATION -------\n");
// Initialize I2C bus.
DEV_I2C.begin();
// ToF initialisation
if(tof_init() == -1) return;
// Indicate end of initialisation
pinMode(LED_PIN, OUTPUT);
digitalWrite(LED_PIN, HIGH);
Serial.println("------- INITIALISATION DONE -------\n\n");
}
void loop()
{
}
/************************** FUNCTIONS **************************/
// ToF initialisation
int tof_init(){
for(size_t i = 0; i < TOF; i++){
// Put all LPn pins to low to disable I2C com.
tab_sensor[i]->begin();
SerialPort.print("Begin sensor #"); SerialPort.print(i); SerialPort.print(" OK\n");
}
for(size_t i = 0; i < TOF; i++){
// Init sensor
status = tab_sensor[i]->init_sensor(address[i]);
if(status == 0) {SerialPort.print("Init sensor OK\n");}
else {SerialPort.print("ERROR INIT SENSOR\n"); return -1;}
// Ranging mode
status = tab_sensor[i]->vl53l7cx_set_ranging_mode(ranging_mode);
if(status == 0) SerialPort.print("Ranging mode OK\n");
else {SerialPort.print("ERROR RANGING MODE\n"); return -1;}
// Resolution
status = tab_sensor[i]->vl53l7cx_set_resolution(res);
if(status == 0) SerialPort.print("Resolution initialisation OK\n");
else {SerialPort.print("ERROR RESOLUTION INITIALISATION\n"); return -1;}
// Start Measurements
status = tab_sensor[i]->vl53l7cx_start_ranging();
if(status == 0) SerialPort.print("Start ranging OK\n");
else {SerialPort.print("ERROR START RANGING\n"); return -1;}
SerialPort.print("Initialisation sensor #"); SerialPort.print(i); SerialPort.print(" done\n\n");
}
return 0;
}The problem is that I can’t initialise my sensors. When I keep the default I2C address for all the sensors, the 1st sensor tries to initialise forever without never returning any error or success code. When I try to initialise each sensor with a different address (0x54, 0x56, …), the init_sensor method returns an error value (value different from 0). I feel like the sensors are not detected at all by the Nucleo board…
Could anyone help me on what I am doing wrong here please?
Thanks a lot!