Skip to main content
Associate
November 14, 2023
Solved

RSVD6 of VL53L5CXV0GC

  • November 14, 2023
  • 1 reply
  • 1242 views

In VL53L5CXV0GC Typical application schematic, The pin RSVD6 must connect a 47 kΩ pullup resistor to IOVDD. If I keep this pin as floating, what will happen? Will power consumption increase? Or is the detection inaccurate?

Thany you.

Dust_huan_0-1699972707833.png

 

This topic has been closed for replies.
Best answer by Anne BIGOT

Hello,
C2 is a Unused GPIO. It's an output so just pull it up gently and ignore it.

You aren't going to use an significant amount of power.

If you are keeping it floating this could damage the sensor or you could get some false measurements.

Best regards
Anne

1 reply

Anne BIGOT
Anne BIGOTBest answer
Technical Moderator
November 22, 2023

Hello,
C2 is a Unused GPIO. It's an output so just pull it up gently and ignore it.

You aren't going to use an significant amount of power.

If you are keeping it floating this could damage the sensor or you could get some false measurements.

Best regards
Anne

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'