Something Wrong with Calibration of VL53L3CX
Vl53l3CX works well when i init it with DataInit and StartMeasurement Function,but when i add a OffsetCalibration to its init sequence,it output a distance of 8191 mm,which is obviously wrong .Paraments of calabration function are shown in the following picture,is there anything wrong.any advice will be appreciated.