TOF sensors VL53 ranging limitations with ambient light
Hi. We are starting a new automation project that needs to detect distance to objects as small as 5 cm by 5 cm, at a distance from 5 cm up to 200 cm. I have been testing VL53L3CX, and VL53L1 through Satel eval. boards. Connected to a proprietary hardware with STM32F407 micro. All the set up is done using STM32cubeIDE.
As our application is intended to be an indoor device we didn't worry about ambient light at first. But I observed that using the device next to a window, no direct sunlight, max. ranging distance degrades severely to a maximum of 60 cm or less depending on target surface and size. I see max distance will be a challenge for our project. I assume we have a laser power and or sensitivity issue here. I would like to know if you have some advice in order to enable VL53 line of tof sensor to be used here.
Any comments will be appreciated.
Regards
Adele.1