Varying data output of Vl53L1X
Hi,
I am using Vl53L1x for a custom application. When i block the sensor with a black tape, i see that the data from getdistance or get signal rate function drops (increases for signal rate functn) after 1 min drastically. For example on blocking the sensor using get distance function the data initially shows reading of500-600, then drops to 300 range values and after 40 sec it drops to 200 and then to 90-100 after 1 min. I would like to know the reason for such drop and is it possible to obtain consistent reading range.
Thank u