VL531L1 measurements always FF.
I have rewritten the C app for the VL531 in LAIRD SmartBasic in order to drive the VL531 from a BT module (BL652). I communicate OK with the VL531 over I2C but when I sent the start command (and after I get a Data Ready from register 0x31 as shown below), the results I get are FFs and the Range status is 01 (SIGMA problem????), as in following:
VL53L1X Model_ID: EA Reg: 0000010F
VL53L1X Module_Type: CC Reg: 00000110
VL53L1X Mask_Revision: 10 Reg: 00000111
__________________________________________________
Address Verification (0x29) : 29 in: 00000001
Value : 03 in: 00000031
Range Status is : 01 in: 00000089
MSB Distance is : FF in: 00000096
LSB Distance is : FF in: 00000097
Distance mode is : 0A in: 0000004B
Report Status is : 00 in: 0000008A
Result Stream Count is : 00 in: 0000008B
Signal is : FF in: 00000098
SPNB is : FF in: 0000008C
SignalPerSpad is 2000.0*signal/SpNb :
AmbientRate is : FF in: 00000090
AmbientlPerSpad is 2000.0*AmbientRate/SpNb :
ROI Center is : 3F in: 0000013E