VL53L0X GPIO1 and ranging sequence
Hi
I refer to the VL53L0X Datasheet DoclD029104 rev5 page 15 article 2.10 Ranging Sequence.
There not a lot descritption in your document
I need to understant how GPIO1 stay down before the sensor pull it up when init/ranging/housekeeping phase is finish.
hypothesys 1/ GPIO1 is not pulled up, the sensor pull it down, then the sensor pull it up when init/ranging/housekeeping phase is finish.
hypothesys 2/ GPIO1 is pulled up by 10k ohms, the sensor pull it down, then the sensor pull it up when init/ranging/housekeeping phase is finish.
hypothesys 3/ GPIO1 is not pulled down, the sensor pull it up when , then the sensor pull it up when init/ranging/housekeeping phase is finish.
hypothesys 4/ the API pull the GPIO1 down and wait that the sensor pull it up when init/ranging/housekeeping phase is finish.
Thanks in advance for answers