VL53L0X inaccurate off-perpendicular?
I'm using the VL35L0X.ino demo code on an Arduino UNO and a clone VL53L0X sensor. I very carefully measured the off-perpendicular distance measurements obtained from the VL53L0X and compared them to actual tape measure measurements. On average there was about 20mm difference between the two.
Also, the VL53L0X gets a little flaky more than 20-30 deg off perpendicular, reporting a '20' about every 3-4 measurement, making it a bit dubious for real-time measurements unless a 5-10 pt average is taken. Granted, the measurements were being done at 1 measurment per second so I would have plenty of time to average, but...


Anyone else care to weigh in on this issue?
TIA,
Frank