VL53L1X ROI (FOV) adjustment question
Hi team,
I want to detect an moving object using the VL53L1X sensor.
However, there is a problem with the installation angle of the sensor, and we arr looking for a solution.

As shown in the above figure, there is interference from a fixed object between the sensor and the moving object in environment installed at angle of about 60 degree instead 90 degree. But, I want to detect only moving objects, not these fixed objects.
At this time, we ask whether the interference of fixed objects can be avoided by moving the FOV from the default 16x16 ROI & Center 199 to the 16x7 ROI & Center 60 as shown figure. Or, is there another solution?
Also, in ideal case, when the linear distance (D) between the sensor and object is 300mm, and the actual measurement distance (E) will be 600mm. However, since the installation angle is not a right angle, the actual measurement distance is expected to be shorter or longer than this from the sensor's point of view. But, if only a certain value is constantly measured without bouncing, i expected that it will be possible to detect.
It's a situation where can't change current installation, so we need to find a solution in current condition, please help.
Best Regards,
Jiung