VL53L1X-SATEL - Low signal and unreliable readings - any ideas?
Hi all
I've built an oil tank level measurement system following https://www.instructables.com/WiFi-Oil-Tank-Monitor/
The system works very well on the bench, but when installed on my oil tank I'm seeing very low signal levels, especially at low ambient temperatures.
For example:
"rangeStatus":"range valid","peak_signal_count_rate_MCPS":"1.57","ambient_count_rate_MCPS":"0.13",
"rangeStatus":"range valid","peak_signal_count_rate_MCPS":"1.51","ambient_count_rate_MCPS":"0.13"
"rangeStatus":"signal fail","peak_signal_count_rate_MCPS":"1.49","ambient_count_rate_MCPS":"0.13"
"rangeStatus":"signal fail","peak_signal_count_rate_MCPS":"1.38","ambient_count_rate_MCPS":"0.39"
At the moment I have the sensor behind an IR window that came with another VL53L1X sensor.
Has anyone else had success using these TOF sensors with kerosene?
Do you have the sensor directly exposed to the oil vapour?
Many thanks
Kind regards
John