VL53L1X temperature effects
We placed two VL53L1X sensors at 18.6" in our temperature chamber.
Over a 50C swing we saw up to 1.15" of variability. In the images bellow the chamber temperature stabilized around 30 minutes.
The target was a large 24x24 sheet of white nylon 0.5" thick
The sensors were left on the entire time, polled every 10 seconds.
SPAD ARRAY size 8x8
Is there any way to improve this? Is it possible to access the temperature registers on the VL53L1x so we can create a variable to compensate for the temperature induced error?