Skip to main content
Associate II
March 22, 2025
Solved

VL53L4CD Setup Issue

  • March 22, 2025
  • 1 reply
  • 625 views

Hello, 

Apologies in advance for the length of this post. 

I am looking for some advice as I am working on getting a cpp based callback for the VL53L4CD sensor, to do this I have written a file which should perform all the same setup as the driver provided however I am encountering a strange error that I cannot understand.

Link to Github with Code, please see: real_time_drivers/VL53L4CD/VL53L4CD_LinuxDriver_V2.3.2/user/uld-driver for all relevant code

When I run my own file first, it sets the sensor to always return a status of two even if I then run the example executable (menu) provided as part of the the driver example this also returns a status of two. 

 

HOWEVER, if I run these in the other order the sensor range is printed perfectly by my own program. This status will remain the same for any executable ran after the first and will be overwritten. 

 

I have tried to find a conditional statement that might cause this however I have been unsuccessful in doing so and would appreciate any assistance provided.

 

As a side note, I have tried adding in the set range timing which is missing from the current code however, this does not solve the issue.

 

Thanks in advance for any help you can provide and feel free to ask for any further clarification.

Regards,

BruGenie

 

Best answer by Anne BIGOT

Hello 

This ticket has been answered on this ticket :

Solved: VL53L4Cd Init Issue - STMicroelectronics Community

1 reply

Anne BIGOT
Anne BIGOTBest answer
Technical Moderator
April 18, 2025

Hello 

This ticket has been answered on this ticket :

Solved: VL53L4Cd Init Issue - STMicroelectronics Community

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'