VL53L5 init stalls at get offset NVM data
I'm implementing the VL53L5CX ultralight driver on an ATSAM4L. The sensor responds correctly when requesting Device ID and Rev. The init function runs without errors (status = 0) through the loading of firmware and restarting the sensor's MCU. But one of the next steps in the init function is getting the offset NVM data. It writes VL53L5CX_GET_NVM_CMD without error (status is still = 0). Then it polls the sensor, and at that point it returns status = 66.
I have a Total Phase I2C protocol analyzer on it during the entire init process. It reports no errors during any of the transactions. Any ideas? This step is the first WrMulti() call where the register address is not 0 (it's 0x2fd8). So that is a possibility. But the I2C analyzer shows 0x2fd8 being correctly passed to the sensor. So I'm running out of ideas. All help or suggestions appreciated!