VL53L5 Status code 2, when there is no target
Hello,
I have connected a "VL53L5 Satel" board to my Arduino nano BLE board, with modified example code. It works fine with: distance/motion indicator in 4 x 4, continuous mode, ranging frequency 1-10 Hz ( i tried different f). But it only works fine when all the zones have targets. If there is no target at all or partially have targets, I get status code 2 for some zones. the zone number with "Status 2" varies from scan to scan. The explanation of status 2 is " target phase". What does this mean? How to solve it? Thanks for your help!!