Skip to main content
Explorer
January 11, 2024
Solved

VL53L5CX arduino mega 2560

  • January 11, 2024
  • 1 reply
  • 1393 views

I just purchased the VL53L5CX-SATEL Breakout Boards for VL53L5CX

https://estore.st.com/en/vl53l5cx-satel-cpn.html

and i have been trying unsuccessfully to get it to work with an Arduino Mega 2560. 

Does anyone know if it is possible to get it working with the Arduino Mega 2560 ? If not, should it work with an Arduino Due ?

This topic has been closed for replies.
Best answer by Anne BIGOT

The library is not compatible with avr architecture due to the fact that the memory size of the chip is too small. 

But the library should work without any issue with the Arduino Due.

You can find this information on the github community here also

1 reply

Anne BIGOT
Anne BIGOTBest answer
Technical Moderator
January 17, 2024

The library is not compatible with avr architecture due to the fact that the memory size of the chip is too small. 

But the library should work without any issue with the Arduino Due.

You can find this information on the github community here also

Our community relies on fruitful exchanges and good quality content. You can thank and reward helpful and positive contributions by marking them as 'Accept as Solution'. When marking a solution, make sure it answers your original question or issue that you raised. ST Employees that act as moderators have the right to accept the solution, judging by their expertise. This helps other community members identify useful discussions and refrain from raising the same question. If you notice any false behavior or abuse of the action, do not hesitate to 'Report Inappropriate Content'