VL53L5CX GUI shows no list of VL53L5CX.
I purchased P-NUCLEO-53L5A1 including X-NUCLEO-53L5A1 and NUCLEO-F401RE.
And I assembled them and connect to PC, and then I installed its driver and reboot windows 10.
When connecting, the explorer open the mass storage drive (D: (F401RE)).
However, VL53L5CX GUI shows no list of VL53L5CX using X-NUCLEO-53L5A1 as the below
Even after pressing the refresh button several times, the result was the same.
I changed the driver's port number from COM15 to COM2.
It's because COM1, COM3~COM15 were already used.
After this, the result was the same.
When I use X-NUCLEO-53L0A1 instead of X-NUCLEO-53L5A1, VL53L0X_GUI works well.
Even after changing NUCLEO-F401RE with X-NUCLEO-53L0A1's instead of X-NUCLEO-53L5A1's, VL53L5A1_GUI shows no list.
Even after updating ST-Link, VL53L5A1_GUI shows no list.
Even after copying 53L5A1_MultiSensorRanging.bin to D:, VL53L5A1_GUI shows no list.
Why does this happen? Is X-NUCLEO-53L5A1 broken?
Thanks in advance.