Skip to main content
FKara.3
Associate III
October 18, 2023
Solved

VL53L5CX safety for human detection

  • October 18, 2023
  • 1 reply
  • 1115 views

Hello,

I plan to use VL53L5CX to measure the distance between the robot and the user (human) in the walker project. I would like to ask if it is safe or not.

 

Regards,

Fehmi.

This topic has been closed for replies.
Best answer by John E KVAM

Absolutely eye save!

The FDA came up with the standards for laser eye-safety. And the define Class 1 as eye safe.

(Those laser pointers are class 3B - acutally quite powerful.)

ST tests every single device off the production line to guarentee it meets the Class 1 standard.

When you get close to production, contact ST for the laser safety test certificate. We will send it to you along with an FDA accession letter issued by the FDA saying that the devices are acknoledged by the FDA. 

- john

1 reply

John E KVAM
John E KVAMBest answer
ST Employee
October 18, 2023

Absolutely eye save!

The FDA came up with the standards for laser eye-safety. And the define Class 1 as eye safe.

(Those laser pointers are class 3B - acutally quite powerful.)

ST tests every single device off the production line to guarentee it meets the Class 1 standard.

When you get close to production, contact ST for the laser safety test certificate. We will send it to you along with an FDA accession letter issued by the FDA saying that the devices are acknoledged by the FDA. 

- john