VL53L5CX ULD and device power consumption
I see that the VL53L5CX sensor has two voltage supply alternatives, both for the digital part (IOVDD) and the analog part (AVDD).
I am also observing that starting from version 1.3.3 of the ULD driver, we have a function called vl53l5cx_disable_internal_cp(). In my tests, calling this function resulted in a decrease in current consumption via AVDD by approximately 40%, for both 2.8V and 3.3V supply voltages. Additionally, it is worth noting that the silicon temperature also decreases significantly when this function is invoked.
What are the effects of this function and in what cases should it be called? Does its usage degrade the sensor's performance in any way?
Thank you!
Alex