Skip to main content
dmeise
Associate
May 20, 2022
Question

"VL53L5CX_ULD_driver_1.3.1" and "CubeIDE_F401RE_Example" I could compile and run the project but when i try to debug it, I will always end up in the Hard Fault Handler. Has anyone an idea why this is happening?

  • May 20, 2022
  • 1 reply
  • 801 views

..

This topic has been closed for replies.

1 reply

John E KVAM
ST Employee
May 27, 2022

I'm not sure but the firmware in the VL53L5 hates to be re-loaded. if it works and then you try to debug, you might be trying to re download the firmware, without powering down the sensor.

could that be it?

  • john