Vl53L7 ranging result distance not correct with status 6
Hi guys, I'm using vl53l7cx without cover glass.
I use the Example_1_ranging_basic in VL53LMZ_ULD_API driver, but i alway receive the result with target_status 6 and the result's distance_mm seem not correct.
Eg i put an target about 300mm in front of the sensor and get result as below in resolution 4x4:
1168-6, 1348-6, 1302-6, 1243-6
1213-6, 1371-6, 1330-6, 1249-6
1240-6, 1381-6, 1332-6, 1253-6
1215-6, 1360-6, 1317-6, 1248-6
So i wonder if i miss any config to get the correct ranging result?
Thanks.