VL53L7CX Some zones not updated fast enough
We are trying to use a VL53L7CX sensor for a people counting application, but some zones won't change fast enough after a person passes through the detection field, even after a long time like 2-3 seconds. I tried resetting the sensor after each ranging, but this also takes too long (more than 1 sec). I'm using it as a 8*8 sensor and a ranging frequency of 15 Hz.
Also I'm using an esp32 as micro-controller and SparkFun_VL53L5CX arduino library, which according to the datasheet of the sensor, should be compatible with the VL53L7CX version.
Does anybody has an what the problem is, and how can I solve it?