Skip to main content
Visitor II
June 11, 2024
Question

VL53L8 with nRF52 DK (nRF52832)

  • June 11, 2024
  • 0 replies
  • 991 views

Hello,

I've been working with a SATEL-VL53L8 sensor for a while. For this I've used the L4RZI board and now i moved into the nRF52 board for more tests.

I've been having trouble trying to implement this. I've tried to use the VL53L0 configuration,

(CONFIG_VL53L0X_PROXIMITY_THRESHOLD    and   CONFIG_VL53L0X).

This because i did not find any configuration for the VL53L8 available (besides the one available in the GitHub for the ST32duino (https://github.com/stm32duino/VL53L8CX)).

I've tried examples for the L0, and the L8, including using the one available in GitHub.

Is there any CONFIG for the VL53L8 that can be used for this board (nRF52 DK)?
 
(I've checked examples between nordic-ST regarding the L1 and L0)