VL53L8CX data fakes after some time
I am using the VL53L8CX sensor to measure distances, and I am getting correct values. After some time, the data starts to be sometimes incorrect, while slowly increasing the ratio of incorrect vs correct, until eventually all of the readings are incorrect.
I've noticed that the time it takes for the data to start being incorrect is linearly related to the ranging frequency.
The resolution I am using is 4x4.
When using ranging frequency = 5, it takes 4 minutes for the first incorrect data.
When using ranging frequency = 10, it takes 2 minutes for the first incorrect data.
When using ranging frequency = 20, it takes 1 minute for the first incorrect data.
When using ranging frequency = 60, it takes 20 seconds for the first incorrect data.
Regarding the "correctness" of the data - the sensor is roughly 200 mm from the surface, and the readings I get at the beginning are as follows:
Zone 0: ambient/spad = 2 | nb_spads_enable = 5632 | signal/spad = 1394 | distance_mm = 210 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 1: ambient/spad = 2 | nb_spads_enable = 2304 | signal/spad = 3380 | distance_mm = 228 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 2: ambient/spad = 5 | nb_spads_enable = 2048 | signal/spad = 2950 | distance_mm = 228 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 3: ambient/spad = 12 | nb_spads_enable = 3072 | signal/spad = 2578 | distance_mm = 227 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 4: ambient/spad = 5 | nb_spads_enable = 8448 | signal/spad = 1032 | distance_mm = 228 | range_sigma_mm = 1 | nb_detected = 1 | status = 5
Zone 5: ambient/spad = 2 | nb_spads_enable = 1536 | signal/spad = 3952 | distance_mm = 233 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 6: ambient/spad = 4 | nb_spads_enable = 1024 | signal/spad = 13169 | distance_mm = 224 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 7: ambient/spad = 5 | nb_spads_enable = 3072 | signal/spad = 2735 | distance_mm = 229 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 8: ambient/spad = 6 | nb_spads_enable = 8192 | signal/spad = 947 | distance_mm = 222 | range_sigma_mm = 1 | nb_detected = 1 | status = 5
Zone 9: ambient/spad = 3 | nb_spads_enable = 1792 | signal/spad = 3936 | distance_mm = 231 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 10: ambient/spad = 23 | nb_spads_enable = 1024 | signal/spad = 16233 | distance_mm = 226 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 11: ambient/spad = 13 | nb_spads_enable = 3072 | signal/spad = 2690 | distance_mm = 232 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 12: ambient/spad = 7 | nb_spads_enable = 11008 | signal/spad = 903 | distance_mm = 196 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 13: ambient/spad = 11 | nb_spads_enable = 5376 | signal/spad = 1705 | distance_mm = 223 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 14: ambient/spad = 6 | nb_spads_enable = 1536 | signal/spad = 4642 | distance_mm = 229 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
Zone 15: ambient/spad = 7 | nb_spads_enable = 3584 | signal/spad = 2596 | distance_mm = 234 | range_sigma_mm = 1 | nb_detected = 1 | status = 9
And the incorrect data looks as follows:
Zone 0: ambient/spad = 4422 | nb_spads_enable = 5632 | signal/spad = 2856718 | distance_mm = 849 | range_sigma_mm = 136 | nb_detected = 1 | status = 9
Zone 1: ambient/spad = 4594 | nb_spads_enable = 2304 | signal/spad = 7066646 | distance_mm = 923 | range_sigma_mm = 137 | nb_detected = 1 | status = 5
Zone 2: ambient/spad = 11039 | nb_spads_enable = 2048 | signal/spad = 5849828 | distance_mm = 915 | range_sigma_mm = 140 | nb_detected = 1 | status = 9
Zone 3: ambient/spad = 26038 | nb_spads_enable = 3072 | signal/spad = 5033753 | distance_mm = 932 | range_sigma_mm = 134 | nb_detected = 1 | status = 5
Zone 4: ambient/spad = 12723 | nb_spads_enable = 6912 | signal/spad = 2262562 | distance_mm = 873 | range_sigma_mm = 140 | nb_detected = 1 | status = 9
Zone 5: ambient/spad = 5364 | nb_spads_enable = 1536 | signal/spad = 8380036 | distance_mm = 928 | range_sigma_mm = 142 | nb_detected = 1 | status = 9
Zone 6: ambient/spad = 8794 | nb_spads_enable = 1024 | signal/spad = 26245266 | distance_mm = 893 | range_sigma_mm = 140 | nb_detected = 1 | status = 9
Zone 7: ambient/spad = 12193 | nb_spads_enable = 3072 | signal/spad = 5388355 | distance_mm = 937 | range_sigma_mm = 138 | nb_detected = 1 | status = 5
Zone 8: ambient/spad = 13173 | nb_spads_enable = 8192 | signal/spad = 1946806 | distance_mm = 891 | range_sigma_mm = 138 | nb_detected = 1 | status = 5
Zone 9: ambient/spad = 8286 | nb_spads_enable = 1792 | signal/spad = 8007507 | distance_mm = 934 | range_sigma_mm = 142 | nb_detected = 1 | status = 5
Zone 10: ambient/spad = 45512 | nb_spads_enable = 1024 | signal/spad = 33468210 | distance_mm = 903 | range_sigma_mm = 138 | nb_detected = 1 | status = 9
Zone 11: ambient/spad = 26319 | nb_spads_enable = 3072 | signal/spad = 5362159 | distance_mm = 942 | range_sigma_mm = 137 | nb_detected = 1 | status = 5
Zone 12: ambient/spad = 14759 | nb_spads_enable = 11008 | signal/spad = 1844806 | distance_mm = 781 | range_sigma_mm = 135 | nb_detected = 1 | status = 9
Zone 13: ambient/spad = 24145 | nb_spads_enable = 5376 | signal/spad = 3501811 | distance_mm = 893 | range_sigma_mm = 136 | nb_detected = 1 | status = 9
Zone 14: ambient/spad = 13877 | nb_spads_enable = 1536 | signal/spad = 9363920 | distance_mm = 916 | range_sigma_mm = 137 | nb_detected = 1 | status = 9
Zone 15: ambient/spad = 14995 | nb_spads_enable = 3584 | signal/spad = 5318915 | distance_mm = 934 | range_sigma_mm = 132 | nb_detected = 1 | status = 9
The distance is about 4 times larger in the incorrect data, and from other tests I've done at different distances, the results always seems to be 4 times larger, no matter the distance.
I've suspected the temperature, but I've used an external fan to keep the temperature low, and the result is the same.
Any advice on how to resolve this issue will be highly appreciated.