VL53L8CX Platform Integration with ChibiOS
Hi, I am trying to integrate the VL53L8CX ULD driver with a project that utilizes chibios on an F4 based board.
The TOF sensor firmware seems to be about 86KB. For a transfer of this size, the device fails to setup and use DMA-safe bouncebuffers. I cannot get it to transfer more than 9865 bytes at once. Can the VL53L8CX_WrMulti(...) calls be broken down into smaller chunks as a work around? If I understand correctly, this is using the auto increment feature of the I2C bus. So to further break the VL53L8CX_WrMulti(...) calls, I will have to ensure the address for each call is sent appropriately. So will this work?
//in vl53l8cx_init(...)
status |= VL53L8CX_WrMulti(&(p_dev->platform),0,(uint8_t*)&VL53L8CX_FIRMWARE[0],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x2000,(uint8_t*)&VL53L8CX_FIRMWARE[0x2000],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x4000,(uint8_t*)&VL53L8CX_FIRMWARE[0x4000],0x2000);
status |= VL53L8CX_WrMulti(&(p_dev->platform),0x6000,(uint8_t*)&VL53L8CX_FIRMWARE[0x6000],0x2000);
Instead of
status |= VL53L8CX_WrMulti(&(p_dev->platform),0,(uint8_t*)&VL53L8CX_FIRMWARE[0],0x8000);
Also, what is the purpose of the register with address 0x7fff?
TIA