VL6180V(1NR/1) absolute maximum range
Hi,
I have a project with VL6180X sensor. Moving from first prototype to second revision, I have realized that I have no use for AWS sensor. Therefore I can switch the sensor to the non-AWS having, also cheaper VL6180V. Datasheets of these sensors are almost identical. The datasheet of the V model has a absolute range of 62cm. However, the range register in question is only 8 bits long. The X variant works fine with this, of course since it is not possible to measure mm values greater than 0xFF mm (255mm) with the sensor (acording to the datasheet of the X variant). Is there hidden register somewhere where it is possible to read rest of the data or is there a mistake on the datasheet?
Here is a link to the datasheet in question. It is a download from your (ST's) VL6180V product page. https://www.st.com/resource/en/datasheet/vl6180.pdf