VL6180X I2C adddress detecting but readings are not coming.
Hi Team,
In this post regarding VL6180x proximity sensor, the sensor is detecting the address(0x29) but the readings are receiving as 255 value even the object it detected in front of sensor. for reference purpose go through this code snippet wrote in arduino IDE for ESP32-WROVER-IE.
What might be the problem?
Regards,
#include <Wire.h>
#include "Adafruit_VL6180X.h"
#define SDA 23
#define SCL 22
Adafruit_VL6180X vl;
void setup() {
Serial.begin(115200);
delay(1000);
Serial.println("Starting I2C...");
Wire.begin(SDA, SCL);
delay(100);
Serial.println("VL6180X test");
if (!vl.begin()) {
Serial.println("Failed to find VL6180X");
while (1);
}
Serial.println("VL6180X found!");
}
void loop() {
//Serial.println("hi");
uint8_t range = vl.readRange();
uint8_t status = vl.readRangeStatus();
// if (status == VL6180X_ERROR_NONE) {
Serial.print("Range: ");
Serial.println(range);
//}
//delay(500);
}Edited to apply source code formatting - please see How to insert source code for future reference.