Water level sensing with some challenges
I'm working on a project that requires liquid level sensing with a couple of complications I'm trying to address. The application is measuring levels in a vessel that is about 1.4m tall, so the ranges of interest are about 100mm to 1.5m. The target liquid is water-based, though not necessarily colorless. I've been testing with clear water as that's a worst case.
The challenges relate to packaging. I need to install the sensor in a fitting attached to the lid of the vessel. For various reason, this means I'm in the end of about a 40mm tube, with a ~20 degree field of view. The other problem is that the fitting is at about a 6 degree angle to the surface of the water. I've been testing with a VL53L1X (set to a central 4x4 ROI) and a VL53L4CX, and things are tantalizingly close to working, but not very reliable. This of course works flawlessly if I have the sensor perpendicular to the surface, even at the end of this tube.
Any tips on sensor selection or configuration/calibration/technique would be greatly appreciated. I know the angle is problematic, but the packaging constraints have put us here.
Thanks,
-Zandr