What is the most raw data that can be collected from the TOF sensors like the VL53L1CB or VL53L5CX?
I'd like to get something as close to the total number of counts for each SPAD vs time since the laser pulse was triggered at the highest temporal resolution possible. It is a bit hard to follow what the histogram functions in the driver are doing. Are these bin sizes adjustable, or are the histograms that you can get from the VL53L1_GetAdditionalData fixed in size?
I saw on another post that for the VL53L5CX there isn't an equivalent set of functions in the driver to get histogram data. Is there any chance that will be something that is coming in the future even with limited functionality?