X-CUBE-TOF1 I2C issue with the STM32WL
Hello, I noticed that using the X-CUBE-TOF Package with the STM32WL55JC Nucleo-Board has an issue with the I2C-Peripheral(I2C-2).
This genrates the I2C code in the IDE.
And the Sensor can be derived.
while if I define the Sensor bus IO:
The Generated code is without the I2C
And the Sensor is not discovered.
Is that normal? should I define something to make the I2C code get generated or this is a bug in the CUBEMX-Package for ToF?
Thank you
Amir