Yes your response is overly complex and my compiler had many unresolved problems with it. What I need is a SIMPLE. list of api function calls and .h file written in "C" NOT "C#" SEE BELOW IN DETAILS PLEASE RESPOND ASAP MY TIME IS RUNNING OUT
Yes your response is overly complex and my compiler had many unresolved problems with it.
What I need is a SIMPLE. list of api function calls and .h file written in "C" NOT "C#"
An init section (this will be processed once upon activation)
- What ever steps it takes to initialize the Vl5310x sensor to allow basic operations
- put unit to sleep
Then a "read a single distance value" and load that into The "hand_distance" variable this will occur over and over
- wake-up sensor
- Take distance data
- put unit to sleep
That is all I need. Here are the parameters
processor BGM13P32F512GA silicon Labs
SDA PA0 PIN5 SCL PA1 PIN6
Simplicity 5 development environment
sensor vl5310x device address 0x52
SDA PIN9 SCL PIN10
Please help me with this. i looked at the github samples but they were mostly for arduino or for python operating systems et. I just need a simple listing. please show me which api calls will get this done.
PLEASE include the the above parameters in the api functions.
Thank you so much. My deadline is here and I need to get your part incorporated into our latest designs
Thank You