BLE profiles - multiple sensors active ST BLE Sensor App
Hello,
I have done the MOOC for the stm32wb55 BLE profiles and now I am trying to introduce more BLE characteristics.
I managed to make the sensors work and to transmit them to the ST BLE Sensor app. However I can only have one screen active at a time. So for instance I can either have the temperature or humidity transmitted at a time, but not both at the same time.
I have created a custom template for both of them, and as I said separately they work fine, however I can't figure out how to have both of them at the same time on my ST BLE Sensor app.
Each template has its own UUID(in template_stm.c), specific to temperature and humidity, however I don't really understand this portion of the code from app_ble.c:
/**
* Advertising Data
*/
#if (P2P_SERVER1 != 0)
static const char local_name[] = { AD_TYPE_COMPLETE_LOCAL_NAME ,'T','R','Y','P','I'};
uint8_t manuf_data[14] = {
sizeof(manuf_data)-1, AD_TYPE_MANUFACTURER_SPECIFIC_DATA,
0x01/*SKD version */,
CFG_DEV_ID_P2P_SERVER1 /* STM32WB - P2P Server 1*/,
0x00 /* GROUP A Feature */,
0x04 /* GROUP A Feature */, //0x00040000
0x00 /* GROUP B Feature */,
0x00 /* GROUP B Feature */,
0x00, /* BLE MAC start -MSB */
0x00,
0x00,
0x00,
0x00,
0x00, /* BLE MAC stop */
};
#endifMy transmission works only when I change the mask to 0x00040000 for temperature (the temperature screen in the app and the transmission work fine) or when I change it to 0x00080000 for humidity. How would I manage to have both of them at the same time?
I read the documents associated in their entirety and also I checked the example apps, but I can't seem to figure it out.
Also as a separate issue, when I try to send the data to the pressure UUID, although the code is exactly the same to the other 2 examples, on the app it shows me "Not available".
Does anyone know how to solve these 2 issues?
Thank you,
Bogdan