BlueNRG-2 (BlueNRG-M2SA) + STLink v3 connection
Hello,
I am integrating the BlueNRG-2 module (BlueNRG-M2SA) in a development with an STM32L496VGT6 processor.
Currently I cannot communicate with the BLueNRG module.
I have done all the tests of my code with the STEVAL-STWINKT1 module, and the minimum configuration to initialize the module and make it operational works correctly, however in the new development the module cannot be made available.
I have searched a lot of information on the web, and I think I understand that the default module comes without any firmware, I don't know if this is correct. My native language is not English and I don't know if I interpret the documentation correctly.
Considering this, I have tried to connect the BlueNRG-2 module to the STLink-v3 mini, but without success.
I don't know if the connections are correct.
I would need if someone can guide me.
1- Does the module have any preloaded firmware?
2 - How should I connect the module to the stlink to load the firmware through one of the BlueNRG GUI or BlueNRG-1_2 Flasher Utility utilities?
thanks!