BlueNRG-2 maximum SPI clock
I am currently using a X-NUCLEO-BNRG2A1 to experiment with the BlueNRG-2. I initially set the SPI rate to 1.25 Mbit/s, but later noticed in the BlueNRG-2 documentation that the maximum SPI rate is 1Mbit/s. My question is how strict is this SPI rate limit, and what is the reason for it (hardware limitations, software limitations)? So far, I've run a number of the examples with no noticeable issues at 1.25 Mbit/s. The MCU I am using has a maximum system clock of 80 MHz. Using the SPI prescalers, the highest SPI frequency I can achieve within the 1 Mbit/s limit is 625 KBits/s. I am hesitant to do this because I don't want to potentially limit the bandwidth of the BLE interface. It seems the only way to achieve the 1 Mbit/s rate is to reduce the system clock for the MCU itself (which would affect the entire application). Ideally, if the BlueNRG-2 could run fine at the slightly higher rate of 1.25 MBit/s (as it currently seems to be doing), it would be the best option.