BLUENRG-LP BLE HID KEYBOARD with WINDOWS 10 PC
DK version:BlueNRG-LP DK 1.1.0
chip:BlueNRG-345AC
2 problems of the ble hid keyboard project.
1st, if BlueNRG-LP is not conneted to any device,it keeps going into RESET ,go on and go on.when it connected to one device,this situation stoped.
2nd,BlueNRG-LP can connected to the android device ,and it works well as a keyboard.But when it connected to the Windows (10) PC,connection is OK,but the PC cannot receive the KEY VALUE of the keyborad. And more,I think the PC did not take the BlueNRG-LP as a keyboard device.
Could somebody tell me why,and how do I modify the program?
Thank you very much!