Skip to main content
Associate II
May 17, 2024
Question

BlueNRG-LP support on Zephyr

  • May 17, 2024
  • 2 replies
  • 848 views

A cursory search of the internet shows the Zephyr Community decided not to port the BlueNRG-LP for use with the Zephyr Framework/RTOS.  The reason they gave (in 2023) was: "not planned".  That seemed a bit vague to me.  

Though this is likely a question for the Zephyr Community, I wonder if anyone here can answer why there seems to be little appetite for porting the BlueNRG-LP to Zephyr? I considered undertaking this effort myself but wasn't sure if there is a reason bigger than: "No one has the time or inclination". 

I will try to ask the same question of the Zephyr Community if no answer here.

Jeff

2 replies

JW_itAuthor
Associate II
May 17, 2024
sardo.michele
ST Employee
August 27, 2025

Hello,

may be too late answer, but BlueNRG-LP has been rebranded as STM32WB07 and it is supported by Zephyr now.

Have a look at Nucleo WB07CC — Zephyr Project Documentation

 

JW_itAuthor
Associate II
August 27, 2025

Hello Sardo Michele.

Thanks for replying. 

 

Yes, I had moved on to other things but I greatly appreciate you taking time to respond to this question as BlueNRG-LP questions have traditionally received very, very light response traffic in the ST Community. 

I do not currently have the rebranded ST WB07CC available to me (only the BlueNRG-LP eval boards currently), but will try once I have the new boards.

Thanks again.

JW