Skip to main content
Associate
February 22, 2024
Solved

BlueNRG-LPS HID change made chip restart

  • February 22, 2024
  • 1 reply
  • 1095 views

I change the HIDdescMap to 

uint8_t reportDesc[] = {
    0x05, 0x01,                 // Usage Page (Generic Desktop)        
0x09, 0x06,                 // Usage (Keyboard)        
0xA1, 0x01,                 // Collection (Application)        
0x05, 0x07,                 //     Usage Page (Key Codes)        
0x19, 0xe0,                 //     Usage Minimum (224)        
0x29, 0xe7,                 //     Usage Maximum (231)        
0x15, 0x00,                 //     Logical Minimum (0)        
0x25, 0x01,                 //     Logical Maximum (1)        
0x75, 0x01,                 //     Report Size (1)        
0x95, 0x08,                 //     Report Count (8)        
0x81, 0x02,                 //     Input (Data, Variable, Absolute)            
0x95, 0x01,                 //     Report Count (1)        
0x75, 0x08,                 //     Report Size (8)        
0x81, 0x01,                 //     Input (Constant) reserved byte(1)            
0x95, 0x05,                 //     Report Count (5)        
0x75, 0x01,                 //     Report Size (1)        
0x05, 0x08,                 //     Usage Page (Page# for LEDs)        
0x19, 0x01,                 //     Usage Minimum (1)        
0x29, 0x05,                 //     Usage Maximum (5)        
0x91, 0x02,                 //     Output (Data, Variable, Absolute), Led report        
0x95, 0x01,                 //     Report Count (1)        
0x75, 0x03,                 //     Report Size (3)        
0x91, 0x01,                 //     Output (Data, Variable, Absolute), Led report padding
0x95, 0x06,                 //     Report Count (6)        
0x75, 0x08,                 //     Report Size (8)        
0x15, 0x00,                 //     Logical Minimum (0)        
0x25, 0x65,                 //     Logical Maximum (101)        
0x05, 0x07,                 //     Usage Page (Key codes)        
0x19, 0x00,                 //     Usage Minimum (0)        
0x29, 0x65,                 //     Usage Maximum (101)        
0x81, 0x00,                 //     Input (Data, Array) Key array(6 bytes)            
0x09, 0x05,                 //     Usage (Vendor Defined)        
0x15, 0x00,                 //     Logical Minimum (0)        
0x26, 0xFF, 0x00,           //     Logical Maximum (255)        
0x75, 0x08,                 //     Report Count (2)        
0x95, 0x02,                 //     Report Size (8 bit)        
0xB1, 0x02,                 //     Feature (Data, Variable, Absolute)        
0xC0 ,                       // End Collection (Application)    
 
#if 1
//radial
0x05, 0x01,                    // Usage Page (Generic Desktop)        0
0x09, 0x0e,                    // Usage (System Multi-Axis Controller) 2
0xa1, 0x01,                    // Collection (Application)            4
0x85, HID_RPT_ID_RADIAL_IN,                    //  Report ID (1)                      6
0x05, 0x0d,                    //  Usage Page (Digitizers)            8
0x09, 0x21,                    //  Usage (Puck)                       10
 
0xa1, 0x02,                    //  Collection (Logical)               12
0x15, 0x00,                    //   Logical Minimum (0)               14
0x25, 0x01,                    //   Logical Maximum (1)               16
0x75, 0x01,                    //   Report Size (1)                   18
0x95, 0x01,                    //   Report Count (1)                  20
0xa1, 0x00,                    //   Collection (Physical)             22
0x05, 0x09,                    //    Usage Page (Button)              24
0x09, 0x01,                    //    Usage (Vendor Usage 0x01)        26
0x81, 0x02,                    //    Input (Data,Var,Abs)             28
0x05, 0x0d,                    //    Usage Page (Digitizers)          30
0x09, 0x33,                    //    Usage (Touch)                    32
0x81, 0x02,                    //    Input (Data,Var,Abs)             34
0x95, 0x06,                    //    Report Count (6)                 36
0x81, 0x03,                    //    Input (Cnst,Var,Abs)             38
0xa1, 0x02,                    //    Collection (Logical)             40
0x05, 0x01,                    //     Usage Page (Generic Desktop)    42
0x09, 0x37,                    //     Usage (Dial)                    44
0x16, 0x01, 0x80,              //     Logical Minimum (-32767)        46
0x26, 0xff, 0x7f,              //     Logical Maximum (32767)         49
0x75, 0x10,                    //     Report Size (16)                52
0x95, 0x01,                    //     Report Count (1)                54
0x81, 0x06,                    //     Input (Data,Var,Rel)            56
0x35, 0x00,                    //     Physical Minimum (0)            58
0x46, 0x10, 0x0e,              //     Physical Maximum (3600)         60
0x15, 0x00,                    //     Logical Minimum (0)             63
0x26, 0x10, 0x0e,              //     Logical Maximum (3600)          65
0x09, 0x48,                    //     Usage (Resolution Multiplier)   68
0xb1, 0x02,                    //     Feature (Data,Var,Abs)          70
0x45, 0x00,                    //     Physical Maximum (0)            72
0xc0,                          //    End Collection                   74
 
0x55, 0x0e,                    //    Unit Exponent (-2)               75
0x65, 0x11,                    //    Unit (Centimeter,SILinear)       77
0x46, 0x00, 0x00,              //    Physical Maximum (0)             79
0x26, 0x00, 0x00,              //    Logical Maximum (0)              82
0x09, 0x30,                    //    Usage (X)                        85
0x81, 0x42,                    //    Input (Data,Var,Abs,Null)        87
0x09, 0x31,                    //    Usage (Y)                        89
0x46, 0x00, 0x00,              //    Physical Maximum (0)             91
0x26, 0x00, 0x00,              //    Logical Maximum (0)              94
0x81, 0x42,                    //    Input (Data,Var,Abs,Null)        97
0x05, 0x0d,                    //    Usage Page (Digitizers)          99
0x09, 0x48,                    //    Usage (Width)                    101
0x15, 0x3a,                    //    Logical Minimum (58)             103
0x25, 0x3a,                    //    Logical Maximum (58)             105
0x75, 0x08,                    //    Report Size (8)                  107
0x55, 0x0f,                    //    Unit Exponent (-1)               109
0x35, 0x3a,                    //    Physical Minimum (58)            111
0x45, 0x3a,                    //    Physical Maximum (58)            113
0x81, 0x03,                    //    Input (Cnst,Var,Abs)             115
0x55, 0x00,                    //    Unit Exponent (0)                117
0x65, 0x00,                    //    Unit (None)                      119
0x35, 0x00,                    //    Physical Minimum (0)             121
0x45, 0x00,                    //    Physical Maximum (0)             123
 
0x05, 0x0e,                    //    Usage Page (Haptic)              125
0x09, 0x01,                    //    Usage (Simple Haptic Controller) 127
0xa1, 0x02,                    //    Collection (Logical)             129
0x15, 0x00,                    //     Logical Minimum (0)             131
0x26, 0xff, 0x00,              //     Logical Maximum (255)           133
0x09, 0x24,                    //     Usage (Repeat Count)            136
0xb1, 0x42,                    //     Feature (Data,Var,Abs,Null)     138
0x09, 0x24,                    //     Usage (Repeat Count)            140
0x91, 0x42,                    //     Output (Data,Var,Abs,Null)      142
0x15, 0x01,                    //     Logical Minimum (1)             144
0x25, 0x07,                    //     Logical Maximum (7)             146
0x09, 0x20,                    //     Usage (Auto Trigger)            148
0xb1, 0x42,                    //     Feature (Data,Var,Abs,Null)     150
0x09, 0x21,                    //     Usage (Manual Trigger)          152
0x91, 0x42,                    //     Output (Data,Var,Abs,Null)      154
0x25, 0x0a,                    //     Logical Maximum (10)            156
0x09, 0x28,                    //     Usage (Waveform Cutoff Time)    158
0xb1, 0x42,                    //     Feature (Data,Var,Abs,Null)     160
0x75, 0x10,                    //     Report Size (16)                162
0x26, 0xd0, 0x07,              //     Logical Maximum (2000)          164
0x09, 0x25,                    //     Usage (Retrigger Period)        167
0xb1, 0x42,                    //     Feature (Data,Var,Abs,Null)     169
0x09, 0x25,                    //     Usage (Retrigger Period)        171
0x91, 0x42,                    //     Output (Data,Var,Abs,Null)      173
0x85, HID_RPT_ID_MEDIA_IN,                    //     Report ID (2)                   175
0x75, 0x20,                    //     Report Size (32)                177
0x17, 0x37, 0x00, 0x01, 0x00,  //     Logical Minimum (65591)         179
0x27, 0x37, 0x00, 0x01, 0x00,  //     Logical Maximum (65591)         184
0x09, 0x22,                    //     Usage (Auto Trigger Associated Control) 189
0xb1, 0x02,                    //     Feature (Data,Var,Abs)          191
0x09, 0x11,                    //     Usage (Duration)                193
0xa1, 0x02,                    //     Collection (Logical)            195
0x05, 0x0a,                    //      Usage Page (Ordinals)          197
0x95, 0x03,                    //      Report Count (3)               199
0x09, 0x03,                    //      Usage (Vendor Usage 0x03)      201
0x09, 0x04,                    //      Usage (Vendor Usage 0x04)      203
0x09, 0x05,                    //      Usage (Vendor Usage 0x05)      205
0x75, 0x08,                    //      Report Size (8)                207
0x15, 0x00,                    //      Logical Minimum (0)            209
0x25, 0xff,                    //      Logical Maximum (255)          211
0xb1, 0x02,                    //      Feature (Data,Var,Abs)         213
0xc0,                          //     End Collection                  215
0x05, 0x0e,                    //     Usage Page (Haptic)             216
0x09, 0x10,                    //     Usage (Waveform)                218
0xa1, 0x02,                    //     Collection (Logical)            220
0x05, 0x0a,                    //      Usage Page (Ordinals)          222
0x95, 0x01,                    //      Report Count (1)               224
0x15, 0x03,                    //      Logical Minimum (3)            226
0x25, 0x03,                    //      Logical Maximum (3)            228
0x36, 0x03, 0x10,              //      Physical Minimum (4099)        230
0x46, 0x03, 0x10,              //      Physical Maximum (4099)        233
0x09, 0x03,                    //      Usage (Vendor Usage 0x03)      236
0xb1, 0x02,                    //      Feature (Data,Var,Abs)         238
0x15, 0x04,                    //      Logical Minimum (4)            240
0x25, 0x04,                    //      Logical Maximum (4)            242
0x36, 0x04, 0x10,              //      Physical Minimum (4100)        244
0x46, 0x04, 0x10,              //      Physical Maximum (4100)        247
0x09, 0x04,                    //      Usage (Vendor Usage 0x04)      250
0xb1, 0x02,                    //      Feature (Data,Var,Abs)         252
0x15, 0x05,                    //      Logical Minimum (5)            254
0x25, 0x05,                    //      Logical Maximum (5)            256
0x36, 0x04, 0x10,              //      Physical Minimum (4100)        258
0x46, 0x04, 0x10,              //      Physical Maximum (4100)        261
0x09, 0x05,                    //      Usage (Vendor Usage 0x05)      264
0xb1, 0x02,                    //      Feature (Data,Var,Abs)         266
0x35, 0x00,                    //      Physical Minimum (0)           268
0x45, 0x00,                    //      Physical Maximum (0)           270
0xc0,                          //     End Collection                  272
0xc0,                          //    End Collection                   273
0xc0,                          //   End Collection                    274
0xc0,                          //  End Collection                     275
0xc0,                          // End Collection                      276
 
#endif
};

 

and made HIDdescMapLen  to the uint16_t from uint8_t 

hid.reportDescLen = sizeof(reportDesc);

typedef struct hidServiceS {
/** TRUE if the device supports the
* boot protocol mode. FALSE otherwise
*/
uint8_t bootSupport;
/** Report Descriptor length */
uint16_t reportDescLen;
/** Report Descriptor */

 

but  this change make the chip restart all the time
what's the matter with it?

what should i do to repair it?

This topic has been closed for replies.
Best answer by yyys

question was be solved

just because i donot remind the max len of the report pack
#define REPORT_MAP_MAX_LEN 80   =>    #define REPORT_MAP_MAX_LEN 480

1 reply

yyysAuthorBest answer
Associate
February 22, 2024

question was be solved

just because i donot remind the max len of the report pack
#define REPORT_MAP_MAX_LEN 80   =>    #define REPORT_MAP_MAX_LEN 480