Skip to main content
oriol
Visitor II
June 19, 2017
Question

Bluenrg-Ms always responding 0xff on MISO pin.

  • June 19, 2017
  • 1 reply
  • 684 views
Posted on June 19, 2017 at 15:42

Hi all,

I have 2 different boards for an application i'm developing, i managed to make bluenrg-ms work on one ! but in the other board i send the header and i receive the response 0x02 SPI ready and the size of write buffer and read buffer, but after that all data answered by the module is 0xFF.

So i tried to get  the module that was working to the board that was not working, and the result is that now the 2 modules are doing the same behaviour, responding correctly to the header but always sending 0xFF as response, so application never gets the command complete, my question is if it can be a hardware problem maybe i crash the 2 modules. If anyone on ST knows this behaviour would be nice to have an answer!

1 reply

Leo_Houston
Associate
July 31, 2024

Any update on this issue? Please do if there is a solution since I have encountered the same issue.

 

Leo