Skip to main content
Yk1
Visitor II
September 29, 2020
Question

Bluenrg x flasher tool for SPBTLE-1S module

  • September 29, 2020
  • 1 reply
  • 618 views

Trying to connect SPBTLE-1S module based on BLUENRG-1 to ST-link/V2 programmer using bluenrg x flasher tool. we did the right connections. but still getting this error. Need to know whats could have gone wrong.

Connected N.1 device by ST Link

13:51:28.135: Waiting device to read -> FAILED. (It's not possible to connect to the device)

This topic has been closed for replies.

1 reply

paul19
Associate III
June 28, 2021

I had the same problem with my X-NUCLEO-BNRG2A1 based on BLUENRG-2, connected to my ST-link V2 clone. My mistake was that I forgot to short the J15 jumper, whose name is "boot pin jumper" and whose description is "Boot pin connect to VDD , for wake up device when in sleep". Hope this will help someone.