BlueNRG2 - Bonded device list empty
Hi all,
I'm using for evaluating purpose two NucleoL4 boards w/ X-NUCLEO-BNRG2A1:
- the first one is running the standard firmware working w/ BlueNRG GUI 4.2.0 (v1.2e - DTM SPI v3.3.0). I setup this board as peripheral;
- the seconds one is running NimBLE stack on the NucleoL4 and DTM SPI basic firmware compiled w/ LL_ONLY option (in order to use HCI commands).
Everything is working as expected: NimBLE is able to scan the peripheral / connect to it / execute pairing.
The problem is that after bonding succeed, if I check bonded devices list (on the board running the peripheral role), this is always empty, as shown in the image.
As result, if I try to reconnect w/ LTK key just exchanged I got pairing error due to encryption failed.
Am I missing something? Similar question was already asked but no answer to the problem
https://community.st.com/s/question/0D50X00009XkWrdSAF/bonding-problem
Thanks for the support.
Alessandro Morniroli