Skip to main content
RKore.1
Associate III
March 12, 2022
Question

Buffer error after debug in the variable field there is an error message uint8_t buff_tx[10] = {11,12,13,14,15,16,17,18,19,20}; program was taken from you tube link : https://www.youtube.com/watch?v=xE6GVt7XuJI

  • March 12, 2022
  • 2 replies
  • 666 views

buff_tx Error: Multiple errors reported.\ Failed to execute MI command: -var-create - * buff_tx Error message from debugger back end: -var-create: unable to create variable object\ Failed to execute MI command: -var-create - * buff_tx Error message from 

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    March 12, 2022

    Perhaps you can show or attach your code. The output from the build process, debugging, etc.

    Indicate what STM32 part/board you're actually using.

    Tips, Buy me a coffee, or three.. PayPal VenmoUp vote any posts that you find helpful, it shows what's working..
    RKore.1
    RKore.1Author
    Associate III
    March 13, 2022

    Thanks Tesla

    I attach the project

    Nucleo 429zi

    Regards

    Raz Koren

    RKore.1
    RKore.1Author
    Associate III
    March 13, 2022

    Yes i can send the project

    Can you send an address to send to