Hello! I'm using module Bluenrg-355MT in my project. There is the antenna ACAG0801-2450-T on my board. This antenna transmits enough over a long distance (D>250m). But reception of this antenna is not more than 15m. Is it possible to achieve long range reception with such type of antennas? Have you tested this module with small size chip antennas? Thanks in advance!
To maximise range, you're going to need the best antenna gain you can get.
Also, it depends on the whole transmission path from end-to-end - see "Link Budget"
"This antenna transmits enough over a long distance (D>250m). But reception of this antenna is not more than 15m"
Sounds like the problem is at the other end - you need to turn the power up at the other end!
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.