Question
Connecting BLUENRG-M2SA to a Raspberry Pi
Hi,
I want to conenct the BLUENRG-M2SA to a Raspberry Pi. This needs to be done through the USB connector.
Can I use a USB-to-UART IC to connect to the UART pins of the BLUENRG-M2SA and then flash the software using this?
Also, do I need to connect the reset pin to the Raspberry Pi, when I flash the software.
Thanks.