Skip to main content
Associate
January 23, 2025
Question

Contiki NG on S2-LP: "HTTP socket error: hostname not found"

  • January 23, 2025
  • 1 reply
  • 1787 views

Originally a reply to this - split to a separate thread as it is a different STM32, different radio, and a new question.


Thank you for your answer. I may consider embenet as option. 

Another thing that I'm trying right now is Contiki NG. I use STM32L152 Nucleo and S2-LP. I succesfully ran border router app and udp client. The next thing I'm trying to do is to run some other examples from contiki os repo like http-example. I removed udp-client file and cp[oed http-example.c file instead. I had to do some modifications in Makefile as. I also added 

#define BORDER_ROUTER_SCENARIO 1
#if BORDER_ROUTER_SCENARIO
#include "net/ipv6/uiplib.h"
#define BORDER_ROUTER_SCENARIO_ADDRESS "aaaa::1"
#endif /*BORDER_ROUTER_SCENARIO*/

in the contiki-platform.c 
I have output:


url http://www.contiki-ng.org host www.contiki-ng.org port 80 path /
Resolving host...

But i get the error "HTTP socket error: hostname not found"


So my questions are:

1. Should the end device(now running http-example) be connected to the internet, or some additional modification of the border router is required ?

2. How to resolve the error ?

1 reply

Andrew Neil
Super User
January 23, 2025

Please see this (also this) for how to properly post source code. I've edited  the post for you.

 


@faruk wrote:

url http://www.contiki-ng.org host www.contiki-ng.org port 80 path /
Resolving host...

But i get the error "HTTP socket error: hostname not found"


"Resolving" a Host refers to converting the human-readable text address "www.contiki-ng.org" to its actual IP address.

This is handled by DNS - the Domain Name System:

https://en.wikipedia.org/wiki/Domain_Name_System#:~:text=An%20often%2Dused,locates%20the%20services.

 


@faruk wrote:

1. Should the end device(now running http-example) be connected to the internet


Of course it must be - because:

  1. http://www.contiki-ng.org is an internet site - you cannot connect to it without an internet connection!
  2. DNS relies upon an internet connection.

 


@faruk wrote:

2. How to resolve the error ?


You will need an internet connection, properly configured with a DNS server.

You're going to have to study the Contiki-NG documentation and/or ask on the Contiki-NG community for specific Contiki-NG support:

AndrewNeil_0-1737629522276.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
farukAuthor
Associate
January 24, 2025

Thank you, 

 

I see that tunslip6 creates the tun0 device, but the interface does not have connection. I guess that is the reason why get request fails. Does anybody have experience with this ?

Andrew Neil
Super User
January 24, 2025

@faruk wrote:

Does anybody have experience with this ?


Those who do are most likely to be found in the Contiki-NG community!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.