Skip to main content
MM.25
Associate
November 24, 2022
Question

Currently we are using KS8721CL of MFR : Microchip and we are looking for an alternate part , Could you suggest an alternate part

  • November 24, 2022
  • 4 replies
  • 1078 views

..

    This topic has been closed for replies.

    4 replies

    Peter BENSCH
    Technical Moderator
    November 24, 2022

    Welcome, @MM.25​, to the community!

    The KS8721CL is or was a PHY for 10BASE-T, 100BASE-TX and 100BASEFX, which STMicroelectronics does not have in its portfolio. However, maybe one of the users in the community has a recommendation for you.

    Good luck!

    /Peter

    MM.25
    MM.25Author
    Associate
    November 24, 2022

    Thank you peter

    Peter BENSCH
    Technical Moderator
    November 24, 2022

    You're welcome!

    If the problem is solved at some point, please mark this thread as answered by selecting Select as best for the relevant answer, as also explained here. This will help other users find that answer faster.

    Good luck!

    /Peter

    Piranha
    Principal III
    November 24, 2022

    You are asking for alternates, but have not named a single requirement and have not even told what exactly you mean by "alternate". With such amount of information I can recommend DP83561.