Skip to main content
Gjain.1
Associate II
October 4, 2021
Solved

Does STSW-STUSB005 GUI needs external STUSB device before installing?

  • October 4, 2021
  • 6 replies
  • 1397 views

..

    This topic has been closed for replies.
    Best answer by Winfred LU

    I though you were asking about an additional USB device plugged to the type C port.

    OK then,

    it will work with EVAL-SCS003V1 dongle itself or

    with NUCLEO-F072RB (being the USB data to I2C bridge) + STUSB47 chip.

    6 replies

    Winfred LU
    ST Employee
    October 6, 2021

    It shall be no.

    You need only a NUCLEO-F072RB board and an EVAL-SCS003V1 dongle.

    Gjain.1
    Gjain.1Author
    Associate II
    October 6, 2021

    While installing GUI 005 , Got a warning NO STUSB detected, operation failed. So thought we might need the EVAL board.

    Do we need both the board Nucleo and Eval-SCS003V1 or just one will work?

    Thanks for answering

    Winfred LU
    Winfred LUBest answer
    ST Employee
    October 6, 2021

    I though you were asking about an additional USB device plugged to the type C port.

    OK then,

    it will work with EVAL-SCS003V1 dongle itself or

    with NUCLEO-F072RB (being the USB data to I2C bridge) + STUSB47 chip.

    Gjain.1
    Gjain.1Author
    Associate II
    October 6, 2021

    Nucleo board is required to customize the NVM through I2C

    EVAL-SCS003V1 is required to customize the NVM through CC pin. Mentioned in the datasheet.0693W00000FBa5sQAD.pngWe could select any one of these based on user requirement.

    Hope you got my query.

    thanks

    Winfred LU
    ST Employee
    October 6, 2021

    The GUI shall also work without any electrical connection to STUSB4761 IC, allowing user to, for example, customize NVM settings and export to a file.

    The warning of "No STUSB detected" is showed when performing operations that require STUSB4761 IC physically, such as "Read IC" or "Flash IC".

    Gjain.1
    Gjain.1Author
    Associate II
    October 6, 2021

    Thanks for your time.

    It means I can still install GUI without any Board in picture. I will try again to install GUI 0005 as last time it didn't happened due to warning issue,